1. I have to get 2.5V output with input 2.9v to 5V max. Will TPS715-2.5V fixed ouput will work fine for load 5mA max.
2. Is there any better LDo for above specs.
3. i checked TPS782. Is it avaialble at fixed 2.5V. If yes, I think it will suit above specs & better than TPS715xx as lower Qcurrent.