This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can BQ24071 work without battery?

Other Parts Discussed in Thread: BQ24071

Dear all,

        BQ24071 is configured AC mode, and TMR is connected to Vref, Rdppm is set 36k ohm, IN power is 12V, battery haven't been connected to the BAT.

        Three tests is done as follow:

        1. Load is 40 ohm, the STAT1 and STAT2 is flashed in turn. And OUT is 6V.

        2. Load is 20 ohm, the STAT1 and STAT2 is all off. And OUT is 0V approximately.

        3. Load is 30 ohm, the STAT1 and STAT2 is all off. And OUT is 0V approximately.

        These means the load current is only 150mA, while the datasheet gives 2A.

        Would you please give me a solution about this, thanks.