HI,
To increase output current, is it possible to cascade LMZ12008 and LMZ12002 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I am wondering if you are attempting to end up we 10A output current capability when you say "cascade". The LMZ 12008 and LMZ12002 are not designed for current sharing applications. If you are looking for 10A output current look at the LMZ23610 or the LMZ22010.
Alan MArtin TI-SVA.
Hello,
That is right, I want to get 10 A output current. As I already use LMZ 12008 and LMZ12002, I was wondering if it was possible to do current sharing. What is the parameter described in the datasheet which indicates if current sharing is possible or not ?
Thanks,
Hello again,
The module devices that accomplish current sharing have a "share" piin and application notes in the data sheet that show how to use them.
Alan Martin TI-SVA