This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610 Charge current does not match what is specified by ISET1



Hello-

I have a resistor divider set up so that I am inputting 0.3V into the Iset1 pin (I verified it). With a sense resistor of 0.010 ohms this should yield a charge current of 1.5A.  What I measure and what is reported by the gas gauge is approximately 980mA of charge current.  Any idea why this is?? 

I thought the current might be being throttled by ACset but I have no load attached and if I attach a load the current does not change. 

The charge cycle should be in constant voltage range since it hasn't reached the charge voltage of 12.6V so the current should be at full strength and not be tapering down.

Any insight on this would be appreciated

-Ray