Dear All,
I am trying to build PFC with UCC28070, I have only first version of PCB and I already know that my layout isnt good enough and need to be rerouted. But even with this i should be capable to findout where is problem with my design. According to my scope measurement it seems that IC is periodicly reseting it self but for now i dont know why?
Channel 1 is SS pin
Channel 2 is VAO pin
Channel 3 is VINAC pin
Channel 4 is IMO pin
This design was created according to you xls file for correct selection of component values.
Parameters of PFC 1500 W, Uout 400 V, external synchronization at 200 kHz (generated frequency is 400 kHz)
Test conditions: Uin 85 VAC, Uout 400 V, Rload=20 kohm (with smaller resistance output voltage starts to fall down)
During normal conditions is PF over 0,9, but it is highly lowered during reset condition.
I am sorry for so much interference in this picture, but my probes are with large signal loops and some signals are deformed because of layout. (tested by probe with small signal loop)
According to
Thanks in advance for any suggestions.