I'm working on a TPS54260 based PS for a cell modem and MSP430 design. I have followed carefully the SLVA412 app note and also read lots of other notes (both TI and others) on the compensation, ceramic cap derating etc.... I found that switchpro seems to fight trying to do things that are more than cookbook so I have a spreadsheet to do all the component and compensation calcs. I verified results against examples.
The design follows the SLVA412 with the exception of needing a 5V output for the modem. I created a test board for the power supply that was a second pass design. The first was also for a wide DC input, but only powering the MSP and I/O. To facilitate tests I did the isolated test board with good test points and cap options. I also setup an MSP430 controlled MOSFET load switch to enable testing 0.15A to either 1A, 2A or 2.5A steps.
After all the research and planning, the transients were much higher than expected. I started with 4 47uF 16V ceramics which even with 40% derating should have been 3x plus what the calculations show is needed (57uF with 0.15A to 2.5A step, 580k Fsw, 10uH L). That got me about 200mV undershoot and overshoot. I went way up to 3x 100uF 10V ceramics and got to ~175mV.
I saw some other posts\replies on someone working on a 4.2V GSM supply and the comments surprised me (starting with 300uF and moving up to 680uF ??)
Why such huge deviation from the calculated requirement (including DC bias derating which i accounted for) ?
Since this supply is meant for outdoor use, I am concerned about 100uF ceramics. If I move to an electrolytic, it's not clear to me on some of the compensation components calcs. I did one experiment with a low ESR 2200uF cap and it was much less clean though I did get to about 172mV. Adding a 47uF ceramic cleaned things a bit, but I think this throws out all of the comp calcs.
So my main 2 questions: Why such large output cap calculation deviations? Is there something I missed that would have given better starting point values?
And: If I decide to use an Aluminum, maybe an Al organic (there are some relatively low cost ones), what are the starting point values, voltage derating and comp calcs I should use?
Thanks,
Christopher Leidigh