This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reliability Request for LM5050



Can you please provide any reliability information for your LM5050.

I checked the on-line tool but no information is available.

If possible please provide the following Info:

•    Total Device Test Hours
•    Number of Failures
•    Burn-In Temp
•    Activation Energy

Thank You

  • Checking into this now.

    Typically, the Reliability Information for SVA devices is located at the very bottom of the 'Sample or Buy' page.

  • Hi,

    LM5050 process reliability metrics is provided below:

    •    Total Device Test Hours = 2,701,916
    •    Number of Failures = 0
    •    Burn-In Temp = dependent on device
    •    Activation Energy = 0.7eV
    •    Failure Rate = 1.3 FITs
    •    MTTF = 766676042 hours
    Failure rate and MTTF were calculated at 60% confidence using the Arrhenius equation at 0.7eV activation energy and derating the assumed stress temperature of 150°C to an application temperature of 55°C.

    Thanks.