Other Parts Discussed in Thread: BQ2000
Hi,
Can I use bq2000 /T with USB source input to charge 3 cells Nicd, NiMH, or 1 cell Li-Ion 3.7V.
Cuongdka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
if the cell capacity is less than 1500mA hours, otherwise the charge current will not be high enough to cause a detectable temperature rise.
Hi Charles,
The source does not matter...the point is that one has to have enough charge current to get a good termination and I recommend at least C/3 to get a good termination circuit.......so yes, USB is good for 500mA so the USB should not be used if the capacity of the cell is over 1500mAHr.