This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150 VEN_HYS tolerance

Other Parts Discussed in Thread: LM3150

Hi team,

I have one question regarding VEN_HYS torelance.
I'd like to know min value and max value. 


Regards,
K.Inagaki

  • I asked another engineer to see if they have the information.  They were going to get back to me later this week.

     

    Regards,

    Marc

     

  • Values for the LM3150 from one lot.

    EN Rising Threshold

    Mean 1.22

    Min 1.204

    Max 1.227

     

    EN Falling Threshold (The rising threshold minus the falling threshold sets the hysteresis)

    Mean 1.09

    Min 1.036

    Max 1.125

     

    You can see that the max of the falling threshold is 79mV below the min of the rising threshold.  This isn't to say that this is the minimum on the hysteresis because those two numbers were not measured on the same part.

     

    Regards,

    Marc