Hello.
Telechips' TCC8925 integrates the ARM® Cortex-A5 core, Mali400 GPU, Ethernet 10/100/1000Mbs, 1x USB OTG, 1x USB Host, 1x SD 3.0 interface, 533MHz DDR3 SDRAM and up to 2Gbyte addressing. RGB/TTL LCD, HDMI and LVDS 8/16-bit EHI interface, 8/16-bit NAND, up to 4 Chips at a time 3 Transport Streams camera in 4 video input controllers. Audio includes SP/DIF as well as AC/97 and 7-channel I2S.
Specification of TCC8925 is download from http://www.winchen.com.cn/upload/file/120607010649.pdf
When I was searching the devices at TI's PMU selector tool page for Processors (http://focus.ti.com/analog/docs/refdesignovw.tsp?familyId=64&contentType=2&genContentId=34106), I was unable to find the Telechips' devices.
Questions:
- Does TI have some suitable PMU devices for TCC8925 ??
- Does TI have a plan to release the PMUs for TCC8925 ??
- Those PMUs is also need to I2C control.
Thanks... C.W.