I am looking for a fast transient response DC-DC switcher that can generate 1.5A out at 5v, given a 6-20v input? Also would like to find a part that could run off of a single Lithium Ion Battery from 2.5v to 4.2v and generate the same 5v @1.5A..The 1.5A is running a RF modem so it would normally be 100ma or less but spike when transmitting. I looked at some specialized TI Power Amp DC-DCs but didn't see anything in that range that would have fast transient response..
Any suggestions?
Charles