Sir/Madam,
I'm trying to use the TPS7A7300 simulation model in Cadence PSPICE 16.5 (with the AMS simulator option) and I'm running into a few issues. When setting the model to an output voltage other than the simulation default using the pin selection method it appears I cannot set the device below ~1.2V. Additionally, I attempted to apply a dynamic load (current step load) to the output of the supply and the output voltage changes dramatically (~200mV) for the duration of the step -- essentially mirrors the shape of the current instead of having a leading and trailing transient. Are you aware of any issues with this model?
Thank you,
Mark Panzer