Hi,
I have a single UCD9222 connected to a single UCD7242. The UCD7242 is providing two separate power rails.
My question relates to how I should wire the UCD7242 TMON signal to the UCD9222. Should the TMON be wired to both TEMP1_AUXADC1 and TEMP2_AUXADC2 pins of the UCD9222? The C6678 EVM does this. However the example schematic in the UCD9222 datasheet (Fig3) only wires TMON to TEMP1_AUXADC1 and the other is pulled low by a resistor.
When using Fusion to monitor the two rails it shows two different temperatures for the UCD7242, one for each rail. Does Fusion know that both rails are on the same UCD7242? Or does it display the values read back from TEMP1_AUXADC1 and TEMP2_AUXADC2?
Cheers,
Richard