I may have hit a slight problem with the power up/dn sequence of the TPS65217C (for AM335x with DDR3), even though it's the prescribed PMIC. It could just be an interpretation problem of the processor's datasheet. Do the dashed vertical lines in figures 4.1 to 4.5 (pages 91-95) of the processors198-page datasheet (SPRS717C) indicate a region where 1v8 and 1v5 can come up in either order? If so it could be better drawn, if not there's a problem as the PMIC's 1v5 DDR3 rail beats the 1v8 rail.
I have spotted several mentions of avoiding more than 2v difference between the ramping up/down of 1v8 and 3v3 regions, if this also applies to 1v5 & 1v8 then obviously it's met, but this isn't a stated requisite.
Using the TPS65217C with an Am335x and DDR3 we get:
PMIC order
|
PMIC
regulator
|
voltage
|
Processor use
|
1st | LDO1 | 1.8v | RTC |
2nd
|
DCDC1
|
1.5v
|
DDR3
|
3rd
|
LDO3
|
1.8v
|
VDDS_PLL CORE_LCD
VDDS_SRAM_CORE_BG
VDDS_SRAM_MPU_BB
VDDS_PLL_MPU
VDDS_PLL_DDR
VDDA_1P8V_USB0/1
VDDA_ADC
VDDS
|
4th
|
LDO2
|
3.3v
|
VDDSHVx
VDDA_3P3V_USB0/1
osillator module etc,
|
5th
|
LDO4
|
3.3v
|
other peripherals:
Ethernet Phy, FLASH etc
|
6th
|
L2, L3
|
1.1v
|
VDD_CORE & VDD_MPU
|
Hope someone knows the answer?