I am evaluating the bq34z100 using the bq34z100EVM and accompanying software and I find that the allowed design energy is very low. The max allowed design capacity allowed by the software is 32767mAH and this is fine for my application since we have a 28 AH battery pack (14s10p configuration). Our voltage is 48 V nominal and 59 V max. This means our expected design energy is at least 48V * 28 AH = 1344 WH. However the allowed range for the design energy is only 32767 mWH (i.e. same a as for design capacity). Even if I assume x10 mode the design energy is far short the needed 1344 WH.
Is there a work-around for this? Can we ignore the design energy setting or will this affect the internal algorithms? I am still familiarizing myself with the functionality of the bq34z100 and want to make sure I don't get stuck later trying to make it work with a 14 serial -10 parallel pack.