This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NEED INFORMATION-TPS63030DSKRG4

 

Can you please provide the following information for the TPS63030DSKRG4 Part ?

1. Typical Power, (Pd typ)

2. Maximum Power (Pd max)

3. Thermal Resistance Junction to Board (Theta JB)

4. Weight

Regards,

Jayakumara K

jayakumara.krishnasetty@honeywell.com

Tel:   +91-80-26588360   Extn: 50116

  • Hi Jayakumara,

    1. If by Pd you are referring to Power Dissipation then,   you can easily calculate Pd from the efficiency curves, figures 3 - 12, in the datasheet. If you are referring to the output power then, that will heavily depend on the Vout, Vin and Iin available. Please refer to figures 1 & 2 and see if that answers your query. 
    2. Refer to answer 1. 
    3. I do not have the theta JB parameter for our board. You can easily measure your Psi JB by following the instructions in this app note: http://www.ti.com/lit/an/spra953b/spra953b.pdf. You can back estimate theta JB by using equation 9. For designing your PCB board please refer to http://www.ti.com/lit/an/snva419b/snva419b.pdf.
    4. 15.165 mg/unit