Sorry I find out that I posted the wrong palce so I post again here. = ="
Hello,
I want to use TPS40211 to make three converters from 12V input to 24V output, 120W full loading and operating in 100K, 300K and 600KHz respectively. I use the exsample circuit on page 26 of datasheet. And it turns out that the 600kHz one can load about 96W (6 ohm, if load heavier like 5ohm then the IC won't drive the Gate of transistor anymore with output only 12V), but the other 100k and 600kHz ones only about 30~40W.
The followings list what I have checked :
1. DIS/EN pin : didn't go over 1.2V (max. about 700mV).
2. Overcurrent sense pin : about 1.1V. But it always about the same value from no load to the limit.
So I have a few questions :
1. I think it's the compensation problem happened on the 600kHz one, but I'm just unable to tune the right result.
2. Is TPS40211 can also work in 100k and 300kHz? or if I misunderstand its spec?
3. I'm not really sure the Fig 2. of the datasheet (page5) meaning exactly. I guess it means,for example, when operating in 600kHz, wit can be during 0.2~0.9 duty cycle, is that correct?
4. Is there other factor that would cause the IC shoutdown I didn't notice?
Please help and thank you.
Regards, shiu