Hi,
I want to use TPS54231 12V input, output required is 5v, 1.4A.
Power loss in TPS54231 is arround 1.7W, I need to operate this device in loco ambient 55°C.
Please specify how many thermal vias are required & Copper area in the PCB required for heat dissipation, off course junction
temperature should not exceed 85°C.
Regards,
SrinivasaPrasad.