Other Parts Discussed in Thread: TPS51200EVM
Hi,
I want to use TPS51200 1.5V input, output required is .75V/1A Used to power DDR3 interface with C6678 processor.
Power loss in TPS51200 is around .8W, I need to operate this device in loco ambient 55°C.
Please specify how many thermal vias are required & Copper area in the PCB required for heat dissipation, off course junction
temperature should not exceed 85°C.
Also specify alternate devices if this device not suitable for above requirements.
Regards,
SrinivasaPrasad.