Hi,
I am using BQ24074 Li Ion battery in my application. I have designed the charger IC to charge the battery at 800mA to 1.3A. But I am seeing the maximum charging current is 200mA. I tried changing ISET, ILIM and ITERM resistors but also it is not affecting much.
I am Using External wall adapter of 5V @ 1.5A
I am using EN1=Low and EN2=High.
currently my ISET= 1.1K , ILIM = 2K and ITERM = 1.18K
Can you please give me the exact tested values of ISET, ILIM and ITERM. So that I can use the same to aceive the below mentioned output
I need an battery to charge at 800mA or More.
Please help me to solve this issue ASAP.
Regards
Nanda Kumar M