Battery Management
[ Battery Chemistry Li-Ion]
[ Battery Capcity (mA-Hrs) 5300mAh]
[ Max Output Current (mA) 2000]
[ Max Input Current (mA) 2000]
[ Max Charge Current (mA) 2000]
[ Min Charge Current (mA) 50]
[Problem:
Hello, I'm using bq20z65 gas gauge in our BMS. We would like to automatically flash the LED display when the [RCA] flag is set in the battery status.
It seems that is possible to set the flag [LEDRCA] in the Operation Cfg B, in the Tab configuration of the Data Flash.
But actually it doesn't work: the LED Display start to flash only with a transition of the DISP pin of the IC.
Thank you for your cooperation, looking forward to hearing from you
Best regards
Mauro Vignali