Hi,
I have done a PCB with a TPS63020 who delivers 3.3V under Vin=4.2V.
I measure a drop, off 100mV when the load takes 1.05 A. ( Vout = 3.3V , when Iout=50mA and Vout=3.2V, when Iout=1050 mA )
Measurements on the evaluation board shows a drop, off only 20mV.
You can see my schematic, board and component placement. Is there possible the problem come from the placement of the capacitors on Vout ?
Thanks you.
Vbr