This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23753AEVM-003 overheating R15 and D7

We have an exact duplicate of the TPS23753AEVM-003 schematic on our custom board. Input voltage over ethernet is 48V and output voltage is 5V @ 1.1A.

Although the circuit is working and producing a clean 5V supply, we find that the 4.7 ohm resistor R15 is getting very hot as is D7. Further investigation shows that the output of the HA3802-AL pin 7 includes a 100ns transient voltage spike which reaches about -30V. D7 conducts to protect the MOSFET as intended so a significant voltage drops across R15. I estimate from the area of the voltage spike on the scope that R15 has to dissipate 6W during the spike and 80mW on average which is above the rated 1/16W in the BoM. This would seem to explain why it is so hot.

I have ordered a TPS23753AEVM-003 to see if it exhibits the same behaviour but it will probably take a week to arrive in the UK. While I'm waiting can anyone shed any light on what might be happening? Can anyone confirm if the EVM shows the same behaviour?

Many thanks,

Alex