I'm working on a 5V to 10 V boost regulator. The normal load will only be 4mA. I need short circuit protection / current limit. So I set the I out to 10mA in the webench table.
The webench designer is requiring a 220uF Electrolytic capacitor for Cout.
I'm curious as to why Cout has to be so large. I have a handful of other designs [granted, other regulator chips, and buck mode] that are converting amps of current that require less capacitance.
I'd prefer to use ceramic caps, but they are much lower ESR. We have had trouble with the bigger SMT electrolytic caps - as far as having them broken off the PCB in shipping. Unlike our usual products, this particular one will be installed in big trucks. If we do have to use an electrolytic, we'll probably use a through hole part.
I'm thinking I'm going to have to do some experiments to see what will work. Any hints about what's more likely to work would be helpful.
Thank you,
Dave
Another question, The feedback resistors are 698K & 100K. Is there any reason I shouldn't make both of them 10 times lower? 6.98K 10.0K