hi
we are engaged in repairing laptop batteries by restoring gas guage original configration ie cycle count, manufacturer date, fcc restored to original. we are facing problems like battery droping from 50% 40% 30% to 6%.can any one have solution to this problem. i would like to mention that batteries can give 1 hour time at 0% which is astonishing. can any one correct this bug in capacity alarm setting. i can send u sbs and data flash images of battery.
thanks