I am using the TPS56121 part in my design with the following requirement.
Requirement:
Vin(min) – 11V
Vin(typ) – 13V
Vin(max) – 13V
Vout – 1V
Iout(max) – 9.5A
I am using the switcherpro tool for designing the circuit. In that the inductor value is 1uH. If I am calculating the inductor value by using the formula given in the datasheet(Page-16), I am getting 64.7nH value. Which value I have to use. Please provide the guidelines to finalize the value .