Hi to all,
I have an application where the battery has to charge supercaps if the voltage of the supercaps drops bellow Vmin (1.5V). I need a buck converter that can enter in shotdown mode or can disconnect himself when the supercaps are fully charged. The Vin is in the range of 3.7V to 4.2V. Is there a component who can do that?
Regards
Gastón
PD: Move this post if this is the wrong forum.