Hi all I am currently in the process designing a power supply for an application.
The parameters are as such
Vin = 5.5V to 28V
Vout = 5V
Imax = 2.5A
I got my design almost complete apart that i need to switch the power supply on and off by using a micro-controller pin, I could use a mostfet/fet switch the Vin but i notice
there was a EN pin on the TPS54332, My question is how would i go about it to use it instead of adding more components for the mosfet/fet switch.
The micro-controller pin output is 3.0V and 5.0V (two different devices but they need to work with the same power supply).
If this is not possible could anyone suggest a mostfet/fet switch design to suit this parameters.
Thanks in advances
Chris