Hi
I am designing with TPS71501 that powers a MSP430F2013. The circuit board also has BQ24650 which requires PGND and AGND.
My question is , which one of this ground do I connect the MSP430 and for the TPS71501 ??
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I am designing with TPS71501 that powers a MSP430F2013. The circuit board also has BQ24650 which requires PGND and AGND.
My question is , which one of this ground do I connect the MSP430 and for the TPS71501 ??
Thanks
Hi Marcelo,
The PGND is typically understood as a local "split" ground to the power supply where local high di/dt, noise currents can be somewhat isolated from other sensitive applications. The AGND is used as reference plane for the compensation and feedback circuitry in order to assure an accurate, noise free output voltage. Ultimately, however, both grounds will be connected together somewhere, of course. Your MSP430, since it is a digital device, will be mostly immune to the noise/current issues. Usually there is a common ground plane to which everything is connected including PGND and AGND. Please consult the MSP430 applications group for best grounding practices for their parts.
Bill
Hi Bill
Thanks for your help.
My issue is that because BQ24650 requires 2 ground which are been connected togueter under the termal pad, I am not sure wich ground to tigh the MSP and LDO TPS. I looked over the MSP430 group and did not find anything related to it.
Thanks
Hi Marcelo,
Attach the MSP430 ground to the PGND point nearest to the output capacitor of its power source.
Bill
Hi Bill
What about the LED TPS71501 ? This is the one that is confusing the most ...
Marcelo
Marcelo,
The output capacitor of the TPS715 should also be connected to PGND too. Let me back up, sorry for the confusion. PGND is referred to in various ways. Local PGND is to contain noisy stuff from the switching regulator. But then there is extended PGND that goes to all the other parts that are powered by the power sources. The TPS715 will be associated with PGND.
Bill
Hi Bill
For some reason I don't think the last post went correct. Please see the attached to a copy of it.
Thanks
Bill
Do you see the pictures ? I need to know what ground to connect where , PGNG and AGND.
Thanks
Bill
Please see the page 17 on the sluu444a to understando what I am talking about the grounds ...
Thanks
Hi Marcelo,
Assuming that the TPS715 supplies the 2.8V power to the MSP430 then all those grounds (marked by "?" (?GND)) should be connected together. If the BQ output (VOUT) is connected to +SYSTEM LOAD then the BQ's PGND should be connected to the ?GND.
I am going home early for the weekend.
Regards
Bill