Hi all,
I got problem with Iq (no load current) of TPS54386, I measured and the input current is too high: 20mA with no load in both 2 output pin, input voltage = 12V.
I used SwitcherPro to design this circuit with input = 12V ~ 25V, output1 = 4V/3A, output2 = 3.3V/2A. From datasheet I see the quiescent current is 5mA with open circuit of output inductors, I can confirm that this is right, 5mA with L1 and L2 are not mounted. But it becomes 20mA with L1 and L2 mounted and no load.
How can I reduce this no-load-current? I expect it is less than 5mA. Or can any one suggest me another switching regulator with low quiescent and dual 2.5A output?
Thank you.