Hi All,
I wanted to migrate my design from TPS65232 to TPS65251 as per TI's recommendation. I have a clarification with respect to TPS65251 device:
As per the datasheet the maximum load on BUCK1 is 3.5A and BUCK2/3 is 2.5A. In my design I want to generate the following
BUCK1 - 1.5V@3.4A (Max limit)
BUCK2 - 3.3V@2A (Max)
BUCK3 - 1.0V@ 2A (Max)
The input is 12V and Fsw = 500kHz. Can TPS65251 be used to generate the above supplies and can the package withstand the thermal dissipation? The graphs to do power dissipation estimation in the datasheet dont have curves for 1.0V.
Regards,
Shareef.