UCD9222+UCD7142 combo pack is used to supply core voltages of C6655. On our custom board, there is no 12V rail. We do only have 5V rail on board. So all required power rails are derived from 5V supply.
It would be great help, if anyone throws some lights on below queries.
Do UCD9222+UCD7242 work at 5V?
Has any one done design with 5V and working without issues?
any suggestion /recommendations are welcome.
Regards,
Udaya