We are using the TPS65930 in a battery powered system. We want the device to remain off upon insertion of the main battery, so I believe we can do that using the mask on register STARTON_VBAT. We do want the system to power on if we use the AC adaptor to provide power to the system. I'm not seeing an available Starting Event which would allow this, so we may have to get creative. Perhaps we could use the VBUS detection for one of these events to allow the system to power on.
What I really need to know is if we can tell which starting event caused us to start. Is there a register which would tell us which event caused the system to start?
Thanks,
Nitro_GS_R