This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Balancing stops with no apparent reason on BQ78PL114

Other Parts Discussed in Thread: BQ78PL114

Hi,

I'm using the BQ78PL114 to manage a 4 cells battery pack.  Actually, my BMS is not able to stabilize the cells.

When my pack is on the charger, the mosfet open when cell1@3.35V - cell2@3.35V - cell3@3.90V - cell4@3.35V.  It is correct because COV is set at 3.9V.  At this point, the balancing is stopped, does someone know why??  The balancing restart when cell4 fall under 3.84V (I found this value doing test - I've not parameter at 3.84V or 0.06V...).  When the cell4 reach 3.8V, the charge mosfet is enabled because COV recovery is set at 3.8V.  And it restarts again and again...

Why is the balancing disabled?  Regarding the spec, I didn't expect the balancing to be disabled in this case.

Thanks

Max