I have a circuit where, since the design released, I have had users whose TPS61030 has failed. This is a low volume design since it is part of a power supply on an evaluation circuit, however the failure rate is quite high, about 5 to 10%. The TPS61030 fails for no rhyme or reason. The TPS61030 itself shorts internally and remains shorted between the input power ( pins 1 and 2 ) and ground ( pins 3, 4, and 5 ). The thermal relief “power pad” doesn’t short though. The short is anywhere from 3 ohms to 35 ohms.
Does anyone have any suggestions as to why this may happen and what I can do to fix this?
I input 3.3V into the TPS61030PWP regulator and have designed it to boost up to 5.0V. The perplexing part about this is that there is little to no current draw on this 5V supply. It was designed to handle at least 300mA of power, but such current draw has never been necessary so typical current draw is theoretically zero, minus any leakage, to possibly 20mA. Due to such low current draw I doubt we can blame this issue on any excessive current. I have had two of these regulators fail in the last week and in neither case was I even using the 5V supply from this part – who knows, maybe that is part of the problem.
I do use the TPS61030 in sycnhronous mode, running at 520 kHz. The clock shouldn't be the reason, it is driving another separate and different power supply and there is no failure there. I have the power supplies synchronized due to this evaluation board's use of RF.
Thanks.