I would like to use UCD90160 to power sequence the C6672 DSP on a board that I am designing.
On the UCD90160, there is a PMBUs and JTAG port. In order to use the Fushion Design GUI provided by TI to program the UCD90160, I believe I would need to use the PMBus to download the configuration file to UCD90160. The JTAG is an alternative to download the configuration file to UCD90160, am I right? If I use the JTAG interface, I would not be able to use the GUI to do the downloading.
Besides monitoring the voltage (eg. when 3.3V goes up, I will output 2.5V_EN to 2.5V regulator), I would also like to have a digital trigger. If input to sequencer goes high (1.8V), I will output 1.8V_EN to 1.8V regulator. How do I do it? Do I use GPI? Or do I use MON pin and set the voltage to be 1.8V?