Hi,
I need help for choosing the right components for the following power system:
Input 1: 28v DC
Input 2: 2/3 Li-Po Cells
Single output: 5v @ 2A
The solution must include an automatic power sources switch, which the 28v DC is the default source in case both power sources are
connected. Also, all the needed protections for dealing with Li-Po 2/3 cells. I don't need a charging circuit (Gas gauge can be nice to have but its not must).
Thanks,
Michael.