Please let me know the three following affairs about the measuring method of DCP020505.
1) Connection of ISO_AGND(Output GND) to AGND or GND will generate heat and damage DCP020505U.
(Grade which it is hot and cannot be touched if it touches by a fingertip)
Please let me know this cause.
In addition, when not connecting with GND, there is no generation of heat.
2) DCP020505U will be generated heat and damaged if GND of an FET probe is connected to ISO_AGND(Output GND).
(Grade which it is hot and cannot be touched if it touches by a fingertip)
It becomes the same phenomenon even if it makes it not connect AC_GND of an oscilloscope.
Please let me know this cause.
3) Please teach me how to measure ISO_+5V and ISO_AGND with an FET probe.
Since DCP020505U heats as mentioned above now, it cannot observe.
In addition, the customer is inquiring by 5Vin / 5 Vout/128 mA.
Thank you for your consideration.