Hello,
We are designing a flyback for 35w output and Vin = 85-265vac.
Do you have pwm controllers with on-chip mosfets for this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We are designing a flyback for 35w output and Vin = 85-265vac.
Do you have pwm controllers with on-chip mosfets for this?
I wouldn't suggest a on-chip FET for 35W in that input range..
The input current i typical too high.
35W/85V = 0.4Arms.. Your peak current in inductor and FET is around 4 times higher than this.. = 1.6A..
This could be your answer: http://www.ti.com/lit/ds/symlink/lm5021.pdf (LM5021). When using a Flyback, use the -2 version since the IC's duty cycle is below 50%.