I need a PD Power Over Ethernet Solution 15W output with an auxillary input of 5V to 12V. I see evaluation boards with aux input voltages much higher than 5V, but I need 5V to 12V. Please provide a solution.
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The lowest practical auxiliary voltage our devices support is 10V.
That is certainly helpful, but for others that have the same question I thing it is important to let them know there are at least 3 methods to provide auxillary power to a PD. One of the methods diode ORs an AUX power source with the PD's output so that the AUX voltage could actually be less than the PDs output which is typically 5V. Here is a link to the document that describes the three methods of implementing AUX power in a PD.
Advanced Adapter ORing Solutions using the TPS23753 (Rev. A)
Application Reports: http://www.ti.com/litv/pdf/slva306a
Sorry, that I didn't completely comprehend the question. Some of our datasheets have a link to this app note on the front page and most have links in the apps section where the adapter solutions are discussed. Let me know if further detail is req'd.