This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Figure 10 and 11 of MC34063A datasheet

Other Parts Discussed in Thread: MC34063A

Figure 10 and 11, these 2 application seems impossible, since during internal switch off, the SW point is at negative level(Vout-Vd), the base of Q1 and Q2 should be kept no 0.7V higher  above that negative level, which seems impossible for the chip to be. Figure 12 is the feasible application of the inverting convert setup. Would TI conside update the datasheet.