Dear Sir,
1. I am using PMP3661 (12-35W) design circuit for 24W - 42V@700mA. In that the current harmonics are 27% at 230Vac and 22% at 120Vac. Please provide solution for improving the current harmonics less than 10%.
2. Whether i can use same circuit for 35W - 36V@1A.