Gentlemen: I've attached the schematic of a BQ24103 design I've used a number of times. This is feeding a 25AH 7.4V Lithium Polymer battery. The max current through the charger is set for about 1.5A, so I removed the cap on TTC to disable the timeout. What I'm seeing is no charge termination. The charger voltage goes up to 8.5V, the battery (no load) is at 8.4, right where it should be, and the current going into the battery has dropped from 1.5A to .3A and is still dropping. But I've run this test before, and the charge never terminates, STAT2 never goes low. Could anyone throw me a clue or give me a list of things to check?