Hi!
I'm trying to run a 3.3V/7A power supply with LM25088MH-1.
As a beginner in power supply design, I tried to keep it simple and use a WEBENCH report as a reference design (Here).
I have changed some parts:
- MOSFET (M1): BSZ097N04LS
- Inductor (L1): SRP1250-4R7M
- Schottky (D1): MBRB1545CTG
- Output cap (Cout): EEE-FP1V331AP
My pcb design is almost the same as the LM25088MH-1's reference design.
When the PSU is turned on with no load, the output voltage is higher than it should be (almost 7V), and when I connect the load voltage decreases. If I connect 1ohm load, the output voltage is 0.5V.
Could someone tell me what should I check or what measurements can I make to solve this problem? I'll use a 100Mhz oscilloscope.
Thank you very much for your help!