This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24630 Q if an adapter can be plugged in all the time and if there are conflicts with output boosting

Other Parts Discussed in Thread: BQ24630

E.G. an emergency light that is wired in a building's main power system but needs to keep a LiFePo4 cell charged. From the docs, it seems this should be okay though the references make me squirm a bit working out how to keep the battery in a happy 2.1V to 3.7V range. I am also trying to figure out where to place a boost as the supply needs to power a 5VDC module.

Like everyone, I'm on a shoestring budget but think I have the charger/supply components about locked down. Btw, thanks for Webench and all the tools you help us with!

Best regards,

Todd A. Kennard