Hi all, i'm Leonardo from Italy
I'm new, and not so expert ^_^
I have 2 questions about ic lm2679
My english is not so good, so i haven't undestand from datasheet what happen if LOAD need more current than what i set with limit resistor. The devide turn off or just limit the output current up to the valor i set?
The second question is about minimun voltage input. My source are 2 lithium cell series configuration, for 7,4V (3,7+3,7). Datasheet says Vin range is 8-40V
Do u think is possible use lm2679 with only 7,4V ?
Are there others IC like this with lower Vin?
Thank you so much for the help. Regards.