This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92210D - PMP3661

Other Parts Discussed in Thread: PMP, LM3464, CC2530

Dear Sir,

i am using PMP3661 design circuit for 24W, 42V @ 700mA, in that current harmonics, ATHD at 230Vac is 27% and at 200Vac is 22%.

Please provide a solution how to improve the ATHD to less than 10%. and the same circuit can i use it for 35W, 36V @ 1A.