The UCC3895 has a minimum operating temperature of 0C. We've had multiple failures of the IC when the temperature is 5C or less. No problems at >5C. My question is why the operating spec of 0C? Should I anticipate failures running at 0C. What is the difference in technology between the UCC3895 and the UCC2895?
A little backgroung.
We only have the problem if the PWM is disabled for a period of time allowing the internal ambient temperature to cool of the power supply to cool to the temperature of the cooling system.