Hello, I'm working with ST's ST1S14 for a 24V-in 5V-out 3A dc/dc. This part is very similar to TPS5450 in pinout, specs and functionality. The problem is the IC enters HICCUP mode at the end of the soft-start cycle with full load connected (resistive load of ~1.5ohm). This is not observed with no load. Also, under short overload transients, the IC occasionally goes to HICCUP mode. In all these cases, the IC should never enter HICCUP mode because of two facts: frist, cycle-by-cycle current limit should act before; second, we measured load current and it never exceeded cycle-by-cycle current limit. I wrote to ST's tech support with no response. I'm thinking about replacing this part with TPS5450, which has almost the same pinout, but I wonder if this part will not exhibit the same behavior.
Do you know if TPS5450 could enter hiccup mode under some cases different than the specified in the datasheet, that is a deep short-circuit that causes overcurrent runaway? I've observed the hiccup current limit is not specified in the datasheet (only the cycle-by-cycle current limit, which is between 6A and 9A). Can you provide min/max values for such current limit?
Thanks.