Attempted to ask this question via Technical Support but I haven't heard anything in a few days so I thought I'd try here.
Question about mode switching in the TLC5926. I am able to switch into the special mode and write to the configuration latch. However, when I use the same process to switch back to normal mode, it fails to do so unless I repeat the process a second time. There is a note in the documentation for this part that states "The signal sequence for the mode switching may be used frequently to ensure that the TLC5926/TLC5927 is in the proper mode." What does this mean? Is it expected that mode switching may fail and the signal sequence should be repeated? How many times should I attempt? Is there a way to know I have succeeded the mode switch?